Stop a Database Instance

You can stop a database instance from running. For example, if you chose an incorrect port for a database instance, you will need to stop that database instance before you can edit the port setting (see Edit or Display the Details of a Database Instance).

To stop a database instance, you can use:

If you are unsure whether a database instance has been registered as a Windows service, view the details of the database instance (see Edit or Display the Details of a Database Instance). If Register as Service is selected, the database instance has been registered as a Windows service.

 

Using the Server Icon

  1. Run the Server Icon for a Database Instance (if it is not already running).
  2. Right-click on the Server Icon to display a context-sensitive menu.
  3. Select Shutdown Server.

 

Using the Geo SCADA Expert Service Manager

  1. Run the Geo SCADA Expert Service Manager.
  2. Select the Stop button for the database instance you want to stop. The name of the service is 'Geo SCADA Expert Server (<database instance name>)'. <database instance name> is the Name defined for the database instance when it was first created (see Add a Database Instance).

 

Using Windows Services

  1. Run Control Panel>Administrative Tools>Services
  2. Right-click on the database instance you want to stop. The name of the service is 'Geo SCADA Expert Server (<database instance name>)'. <database instance name> is the Name defined for the database instance when it was first created (see Add a Database Instance).
  3. From the context-sensitive menu, choose Stop.

Disclaimer

Geo SCADA Expert 2019